TGML Elliptical Arc: <Arc>
Arc defines an elliptical arc. The elliptical arc is part of an ellipse.
                                            
                                        
| Attribute | Type | Description | 
|---|---|---|
| 
                                                         Center  | 
                                                    
                                                         Point  | 
                                                    
                                                         The center point of the ellipse.  | 
                                                
| 
                                                         Fill  | 
                                                    
                                                         Brush  | 
                                                    
                                                         Specifies how the interior of the shape is painted.  | 
                                                
| 
                                                         Opacity  | 
                                                    
                                                         Double  | 
                                                    
                                                         A value between "0.0" (transparent) and "1.0" (opaque)  | 
                                                
| 
                                                         Left  | 
                                                    
                                                         Double  | 
                                                    
                                                         The x coordinate of the upper left corner of the ellipse.  | 
                                                
| 
                                                         RadiusX  | 
                                                    
                                                         Double  | 
                                                    
                                                         The horizontal radius of the ellipse.  | 
                                                
| 
                                                         RadiusY  | 
                                                    
                                                         Double  | 
                                                    
                                                         The vertical radius of the ellipse.  | 
                                                
| 
                                                         StartAngle  | 
                                                    
                                                         Double  | 
                                                    
                                                         Specifies the angle between the x axis and the starting point of the arc.  | 
                                                
| 
                                                         SweepAngle  | 
                                                    
                                                         Double  | 
                                                    
                                                         Specifies the angle between the starting and ending points of the arc.  | 
                                                
| 
                                                         Stroke  | 
                                                    
                                                         Brush  | 
                                                    
                                                         Describes how the line is painted.  | 
                                                
| 
                                                         StrokeDashArray  | 
                                                    
                                                         Array of Double  | 
                                                    
                                                         The pattern of dashes and gaps used to outline shapes:  | 
                                                
| 
                                                         StrokeWidth  | 
                                                    
                                                         Double  | 
                                                    
                                                         The width of the outline of a line.  | 
                                                
| Visibility | Visibility | 
                                                         Specifies if the element is visible or not.  |